AXIS#.IL.COGCOMP.TEACH.POSSTART

Description

The start position needed during the Cogging Compensation teach to achieve a constant velocity before reaching the cogging compensation table minimum position.

Versions

Action Version Notes
Implemented 02-08-00-000

General Information

Type

Read Only

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value 0

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.